{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the list of Replacement Parts needed for an inoperative Hand-Off-Auto on the ATV660 drive?

Issue:

How can I find a list of parts needed to replace the Hand-Off-Auto on an ATV660?

Product Line:

Altivar Process Drive

Environment:

ATV660 Process Drive

Cause:

Hand-Off-Auto is broken or not working

Resolution:

The part list for the Hand-Off-Auto Selector are the following:

(1) ZB5AD3

(1) ZB5AZ103

(2) ZBE102

(1) ZBZ32

(1) 65170-166-17

Schneider Electric Nigeria