{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the connector used to connect LPCTs to Sepam relay?

Issue:
Customer has current connector CCA630 and wants to use LPCTs but can not connect it to Sepam

Environment:
Sepam 20 40 80 measurements

Resolution:
The 3 LPCT sensors are connected to the CCA670 or CCA671 connector on the rear panel of Sepam.
The connection of only one or two LPCT sensors is not allowed and causes Sepam to go into fail-safe position.
The two CCA670 and CCA671 interface connectors serve the same purpose, the difference being the position of the LPCT sensor plugs:
-  CCA670: lateral plugs, for Sepam series 20 and Sepam series 40
-  CCA671: radial plugs, for Sepam series 80.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: