{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
EcoStruxure Machine Expert - How to convert a DWORD variable as a real value with a floating point based on IEEE-754 standard?

Article available in these languages: Spanish

As shown in the picture below, the DWORD_TO_REAL function doesn't allow to convert a DWORD variable as a real value with a floating point based on the IEEE-754 standard.

In order to convert a DWORD variable to a real value following the IEEE-754 standard, we have to create a DUT - UNION type.


DUT definition:
Image1

Image2

Schneider Electric Nigeria

Attachment(s)
DWORD_TO_FLOAT_IEEE-754.project [488.71 KB]