{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to use the PLC simulator

Article available in these languages: Japanese

How to use the  PLC Simulator for EcoStruxure Control Expert.

The PLC Simulator is installed with EcoStruxure Control Expert.  It can be used to
test a Control Expert project during development.

This video will:
  • demonstrate how to create a Control Expert project and test it using the PLC simulator
  • demonstrate how to use the Control Panel for the PLC Simulator.
As a prerequisite, the user must be familiar with using EcoStruxure Control Expert and the M580 PLC.


Schneider Electric Nigeria