{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to configure a Modicon Switch for Port Based IP assignment
The Modicon switch has a feature that allows a user to serve the same IP address to any device connected to that specific port on the switch. This video will demonstrate how to specifically configure the switch when a 170ENT11001 Ethernet Communication Adapter will be connected to the port.
For example, if Port 3 on a Modicon switch MCSESM103F2CS0, is configured to serve an IP address 192.168.1.33, then any 170ENT11001 that is connected to Port 3 will be assigned that IP address.





Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: