{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I use the Unity Loader utility to upgrade the firmware of the BMENUA0100 OPC UA module?

Issue:
Utility used for upgrading the firmware of the BMENUA0100 OPC UA module


Product Line:
M580, EcoStruxure Control Expert, BMENUA0100


Resolution:
No, The Unity Loader cannot be used for upgrading the firmware of the OPC UA module. You must use the EcoStruxure Automation Device Maintenance V2.0 utility. You can download the utility and firmware file from the Schneider Electric public site at

EcoStruxure Automation Device Maintenance V2.0 :
https://www.se.com/ww/en/download/document/EADM/

BMENUA0100 OPC UA module firmware:
https://www.se.com/ww/en/search/bmenua0100?multifilter=Software

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: