{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
BMEAHI0812 FDR Server shows offline

Issue

Transfer to FDR server shows offline

Product Line

BMEAHI0812

BMEAHO0412

Environment

EcoStruxure Control Expert

Resolution

There can be a couple of reasons that the FDR server shows offline. One, you must have an Ethernet connection. You cannot use the USB connection. Another reason could be that the FTP service in security has been disabled. FTP needs to be enabled.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: