{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why am I unable to set "LAR" to DI4 with SoMove when using Master/Slave on a Process Drive?

Issue:
Can you have a Master/Slave configuration set to Slave, and use Limit Switch Positioning with Altivar Process Drives?

Environment:
ATV900 series
ATV340 Ethernet version drives
ATV600 series with VW3A3721 option card

Cause:
A request is in progress to update literature with technical publication team

Resolution:
Limit switch function can only to be configured on the master drive. The slave follows internal RUN order given by the master, then if the master stop because of limit switch function it will stop the slave(s) as well. This is why it is not possible to configure limit switch function on slaves side.

We must keep in mind that our Master /Slave function is a torque or speed follower.
Slaves are only followers and the master controls the whole system in our approach.

Limit Switch function LAF and LAR can only be assigned a digital input when Master/Slave MSID and MSDT are both set to Master.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: