undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to set up Somove to connect to a ATV340 Drive using CANopen.

Issue:

How can you connect Somove using the CANopen connection option?

 

Product Line:

ATV61, ATV71, ATV320 and ATV340 only

 

Environment:

All

 

Cause:

Connection using CANopen

 

Resolution:

You will need to use a CANopen USB-CAN Dongle ( Port 1 only is supported) if you have a dual port.

This connection option is only supported with the ATV61, ATV71, ATV320 and ATV340 Drives only. You can not use this option on the ATV630 or ATV930 drives.

See the attached document on setting up Somove to use CANopen.

Schneider Electric Nigeria

Attachment(s)
SoMove CANopen connection instructions.pdf [674.32 KB]
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.