{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What’s TeSys Giga?
TeSys Giga is the new generation high current contactors and overload relays from 115 A to 800A in 3 frame sizes. It is available in 3-pole and 4-pole in standard and advanced versions. Thanks to wide band AC & DC coil control, the complete range is covered in just 96 product references. Both standard and advanced versions have self-diagnosis feature, with LED function which enables predictive maintenance.
TeSys GigaG115G150G185G225G265G330G400G500G630G800
Ie (AC-3)/440V115A150A185A225A265A330A400A500A630A800A
Ie (AC-1)/ 440V250A275A305A330A385A440A550A700A1050A1050A

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: