{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to interlock contactors in two different sizes of TeSys Giga contactors ?

Article available in these languages: Dutch

TeSys Giga contactors can be interlocked with same ratings or with different ratings. The
various ratings have similar frame sizes and interlocking kits are defined based on the frame sizes.
RatingsFrame size
G115-G225 (115A-225A)Frame 5
G265-G500 (265A-500A)Frame 6
G630-G800 (630A-800A)Frame 7







image.png

Note: Maximum 3 auxiliary contacts can be installed between 2 contactors with mechanical interlock kit.

Schneider Electric Nigeria