{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
MiCOM P12x/y Remote controls not working
Issue
I am trying to send Controls via Modbus RTU to a MiCOM P121 IED but not working.

I managed to read the LED statuses (Add: 12) & Analogs (Add: 48, 50,52,54) 100% correct.

According to manual we need to send commands through Holding register 400 (bit 3 & 4 ) for trip and close orders respectively. I tried that, and I even tried to send a control to bit 2 “Clear all alarms” and still nothing. (injected a trip)

I did assign trip and close to RELAY OUTPUT 3 & 4 on the relay face plate settings,

Any idea what else we can try ?.

_____________________________________________________________
Product Line
MiCOM P12x, MiCOM P12y.

_____________________________________________________________

Environment
Control not works when program mode is active.

_____________________________________________________________

Solution
If reading is fine but writing remote commands are not accepted, the device is in programming mode.
The programming mode is indicated with the letter "P" on the right hand side of the display on each menu heading. The letter "P" remains present as long as the password is active.
Program mode will deactivate when there is no activity on keypad for 5 minutes.
Remote commands will work after "P" letter goes off in the HMI..

_____________________________________________________________

*Warning:  Installation, maintenance, up-gradation, down-gradation of MiCOM device should only be performed by qualified, competent personnel that have appropriate training and experience. Failure to follow the instructions / warnings in the Installation / Operation Guide can result in unwanted disruption to the power system, permanent damage to the device, severe injury or death.*

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: