{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where is the access level in the ATV320 drive?

Article available in these languages: Japanese

Issue:
Not able to find the access level (LAC) parameter in ATV320 drive

Product Line:
ATV320

Environment:
ATV320 all series

Cause:
Trying to find the  LAC parameter in ATV320 drive, but not able to find it.

Resolution:
On the keypad:
Go to ConF, Full and then look for LAC (access level)
Options are:   Basic (bAS); Standard (Std); Advanced (Adv); Expert (EPr).
Expert will allow you to work without restrictions in the drive.

In SoMove:
Go to “Parameters” tab, then go to “Full” in the left side menus and it will show the Access level parameter in the right area.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: