Issue:
What is the POE spec for the NetBotz 755
Product Line:
NBWL0755
Environment:
NetBotz power over ethernet
Cause:
NetBotz 755 requires POE. Not all POE power options are compatible
Resolution:
The NB755 meets the standard for IEEE802.3at and it has a classification resistance of 63 Ohms.
This makes it type 2 device.
A type 3 power supply can also power a type 2 device with no issues.
APC has offered 2 POE injectors:
NBAC0303NA
Power over ethernet PoE up to 18 Watts Supported Products
NBWL0356A
NBWL0456A
EGX150POE
NBAC0303NA2
Power over ethernet PoE+ up to 36 Watts
NBWL0756
IEEE802.3at class 4
(new) (more power)
Also known as Type 2 PoE
What is the POE spec for the NetBotz 755
Product Line:
NBWL0755
Environment:
NetBotz power over ethernet
Cause:
NetBotz 755 requires POE. Not all POE power options are compatible
Resolution:
The NB755 meets the standard for IEEE802.3at and it has a classification resistance of 63 Ohms.
This makes it type 2 device.
A type 3 power supply can also power a type 2 device with no issues.
APC has offered 2 POE injectors:
NBAC0303NA
Power over ethernet PoE up to 18 Watts Supported Products
NBWL0356A
NBWL0456A
EGX150POE
NBAC0303NA2
Power over ethernet PoE+ up to 36 Watts
NBWL0756
IEEE802.3at class 4
(new) (more power)
Also known as Type 2 PoE
Released for:Schneider Electric Nigeria