{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
When the PLC control is used on advanced version TeSys Giga contactors, do we still need to connect A1/A2 ?

Article available in these languages: Japanese

AC or DC control voltage input to A1-A2 is a must and this control voltage defines the proper functioning of the contactor. When the PLC input is ON, the contactor operation can be controlled by the 24V DC PLC signals.

Please refer to the below schematic extracted from catalogue page:


image.png


Schneider Electric Nigeria