{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an tLOF or Drive Overload error on the ATV630 and ATV930 Drives?

Issue:

tLOF error or Drive overload error.

Product Line:

ATV630 and ATV930 Drives

Environment:

All

Cause:

- Ambient temperature too high.

- Bad cooling.

- Filter blocked.

- Check the ventilation.

- Function of fans faulty.

Resolution:

- Verify the size of the load/motor/drive according to environment conditions.

- Check the ventilation of the inverter and the ambient.

- Verify the settings of the [Drive Overload Monit] tLOL parameter.

Schneider Electric Nigeria