{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimum clearance required when installing 2 or more TeSys Giga contactors side by side ? (with or without auxiliary module) ?

Minimum 5mm gap  is recommended as safety clearance between 2 contactors with or without auxiliary contacts, when they are installed side by side.

Please refer to the catalogue page with X2(mm) in dimensions section.

X2 = Minimum distance between the contactor side including additional auxiliary module and other devices like contactor or metallic parts.

5 mm gap between 2 contactors side by side

Schneider Electric Nigeria