{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What temperature does 100 percent THD represent on the ATV630 Process Drives?

Issue:

Ambient heatsink temperature when the THD is 100 percent?

Product Line:

ATV630 Drive

Environment:

All

Cause:

Heatsink temperature if the thd (Drives thermal temp) reads 100 %.

Resolution:

If the THD is reading 100% this is around approximately 85 degrees C.

The drive will trip on OHF at 118% or approximately 100 degrees C or between 90 degrees C to 105 degrees C.

Schneider Electric Nigeria