Search FAQs
What is a Ot fault on a ATV212 drive?
Issue:
Getting Ot fault on a ATV212 drive
Product Line:
ATV212
Environment:
Ot faults
Cause:
n/a
Resolution:
This is a Overtorque fault. The calculated motor torque has reached the level set by Parameter F616 (Overtorque Detection Level)- factory default set to 130%, can increase, if needed.
F615 (Overtorque fault/alarm selection)- can set to 0 for Alarm or 1 for Fault.
Released for:Schneider Electric Nigeria
Explore more
Product:
Explore more
Product: