{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to downgrade the EOTE project?

No, It is not possible to downgrade the EOTE project to an older version.

But when we upgrade the original project, for example, when we upgrade the project from EOTE 3.1 SP1A to EOTE 3.2, EOTE will create a back-up project file. we still can open the back-up project with EOTE 3.1 SP1A. So please keep the back-up project properly if needed.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.