How many maximum auxiliary contact blocks can be mounted on TeSys Giga contactors ?
Maximum 4 auxiliary contact blocks can be installed, means maximum 4NO+4NC contact combination can be achieved. 2 blocks on the right side and 2 blocks on the left side of the contactor can be installed.
Released for:Schneider Electric Nigeria
Explore more
Range:
TeSys Giga contactors
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.