{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PME 2021 - PME EWS data not available in EBO or other application

Product Line

Power Monitoring Expert 2021

EcoXtruxure Building Operation 3.2

_____________________________________________________________

Environment

Data Exchange / System Integration

EWS Server

_____________________________________________________________

Issue

Unable to display EWS data in EBO or any other application.

The application is able to connect to the PME EWS server but it is unable to display any data.

_____________________________________________________________

Proposed Solution

  1. First, ensure that EWS Server is enabled in PME - Configuring the EWS Server
  2. Update or create EWS login in PME - EWS Login
  3. Follow the steps to integrate PME/EBO as described in the PME system guide - Integration with EcoStruxure™ Building Operation (EBO)
  4. Use the EWS Client test to troubleshoot the connection between PME and EWS - FA269362
  5. Open the EWS web.config file located at PME\Applications\EWS - make sure to backup it before editing it
    1. find the line <wsdlExtensions location="http://localhost/EWS/DataExchange.svc" singleFile="True"/>
    2. change the localhost to be the PME server IP address or name
    3. save it, run iisreset in the command prompt (run as admin) and restart ION Application Modules Core service

For testing purpose:

1) Test the EWS URL in the application server and the client server: http://localhost/EWS/dataexchange.svc?wsdl

2) Tool step 4

Note: If the Client is running on the server where PME is installed, then “localhost” can be used. If PME is on a different server, then the IP address of that server must be used. Use the IP address or server name of the PME server in the address http://<IPaddress>or<servername>/EWS/dataexchange.svc?wsdl

it should return a page similar to:

_____________________________________________________________

Additional section

To enable EWS to connect using HTTPS - FA414893

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: