{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an Altivar drive be used to create the correct power system to supply a machine?

Issue:

Can the Altivar drive act as a power supply for non-motor loads?

Product Line:

Altivar

Environment:

All models

Cause:

Applications to change power systems

Resolution:

Altivar drives are designed to power motor loads only. It is a misapplication to use the drive output to power other loads, such as a control transformer, relay coils, resistive loads.

Drives can generally convert single phase power to three phase (check ratings) and will vary the output voltage and frequency to control a motor load.

A drive can power a machine motor, but all other loads on the machine need to have a separate power supply.

Schneider Electric Nigeria