I have to fill out Wi-Fi SSID and Password each time I want to add Wi-Fi device on iOS
For this, you have to have enabled in iOS settings a Precise Location, you can navigate to its option by Settings -> Wiser -> Location after this is enabled the SSID and Password will be filled out automatically
Released for:Schneider Electric Nigeria
Explore more
Product:
CCT501901
Articles that might be helpful
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.