undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to set IP address of a HMIGTO target when using Modbus USB Equipment connection in VJD 6.2 SP11?

In Vijeo Designer 6.2 SP11, we can't set HMIGTO IP address in the same network segment with a M340/M580 PLC when you try to connect the HMIGTO to the M340/M580 PLC via USB. As we know, the default IP address for M340/M580 PLC is 90.0.0.1, which we can't change. So we can't set the HMIGTO IP address as 90.0.0.<example>. Otherwise there will be no connection.

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.