Search FAQs
How to upload and convert a Modicon Micro 110CPU612xx Modsoft application to Unity.
Use the following steps to upload the application using Modsoft:
- Start Modsoft.
- Click on Transfer
- Select 'PLC to File'.
- Select 'New Program'.
- Type in a filename.
- Hit ENTER
- Type in a location for saving the application or just use the default location.
- Hit ENTER
- Type in the Modbus address.
- Hit Enter.
- Select the Modbus I
- Select RTU for the mode.
- Select Even for the parity
- Select the Stop Bit.
- Select the baud rate.
- Select the appropriate COM port on the PC.
- Wait for the upload to finish.
- Save the changes.
- Start
- Open the application with Unity using the 'Modsoft projects' selection.
- Save the Unity application.
- Select the PLC type to convert to:
- Click on OK.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: