{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you use the VW3A1113 mini HMI to finalize the firmware update on the ATV340 Drives?:
Issue:
Use the VW3A1113 HMI to complete ATV340 firmware update.

Product Line:
VW3A1113

Environment:
All

Cause:
HMI is used to finalized the firmware update and its missing menu 7.3.

Resolution:
No you can not use the VW3A1113 HMI to complete the firmware update on the ATV340 version Drive.  The VW3A1113 HMI will not display menu 7.3 which is needed to finalize the firmware update.   You have to use the VW3A1111 to complete the firmware update.

Schneider Electric Nigeria