{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to update the firmware of the Harmony STM6 Edge Box HMISTM6BOXIOT?
The goal of this FAQ is to explain how to update the firmware of the Harmony Edge Box HMI.

This article is applicable for HMISTM6BOXIOT.


To update the firmware of Harmony STM6 Edge Box HMI, need to follow some step (Last official update: V1.1.0).

Here the steps:
1 - Download the last software corresponding to the last official update: https://schneiderelectric.sharepoint.com/:f:/s/BoxSupportL3Group/EiO8SIa0xSVAgsXxTW6XbpEBgNU7lpMDlq0sEBs56UWWZg?e=RHI6zt
2 - Copy BOOTLD13.SYS and BOOTOS13.SYS to root of USB storage.
3 - Insert the USB flash disk in the USB port of HMISTM6BOXIOT.
4 - Connect to the configuration menu.
view

The duration to update the firmware is around 1 - 2 minutes.
After update the target will restart automatically.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: