{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are files with the extension .HMIX?
Issue
Where do files with the file extension .HMIX come from?

Product Line
Vijeo Designer
Intelligent Data Services

Environment
HMI Configuration Software

Resolution
.HMIX extension files are exported from Vijeo Designer HMI applications that are used to create solutions for an add-on called Intelligent Data Services (IDS). IDS is a tool that runs on a Windows Server that is used to comply with FDA Electronic Records and Electronic Signatures standard "CFR 21 Part 11". for the Food and Pharmaceuticals industry.

To perform this export:
1) Right-click on the name of the HMI ("Target1" is the default name)
2) Choose "Export..." from the context menu
Vijeo Designer Target Export
A Validation of the project will occur.

3) Save the file:
Save As screen

Schneider Electric Nigeria