Issue:
It appears that the AI1C, AI2C and AI3C images for the input are not available.
Product Line:
ATV320
Environment:
All models
Cause:
Keypad monitoring of analog input signal
Resolution:
Navigating to the Monitoring menu, IO Map, Analog Inputs image to show the input V or mA signal value is only accessible with a connected graphic display keypad. The integral keypad will show the analog input assignment, but not the input value. Options for a graphic display keypad include VW3A1101 and VW3A1111.
Released for:Schneider Electric Nigeria
Issue:
It appears that the AI1C, AI2C and AI3C images for the input are not available.
Product Line:
ATV320
Environment:
All models
Cause:
Keypad monitoring of analog input signal
Resolution:
Navigating to the Monitoring menu, IO Map, Analog Inputs image to show the input V or mA signal value is only accessible with a connected graphic display keypad. The integral keypad will show the analog input assignment, but not the input value. Options for a graphic display keypad include VW3A1101 and VW3A1111.
Released for:Schneider Electric Nigeria