{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a BMXCPS4002S and BMXCPS4022S redundant power supplies be used together in a redundant rack?
Different redundant power supply models are allowed in the same redundant rack as shown below.  They do not have to be of the same model number.

In this example, a BMXCPS4022S (24-48 VDC input) and a BMXCPS4002S (100-240 VAC input) are installed.
It is normal to have two different voltage sources powering a rack.
BMXCPS4022S and BMXCPS4002S redundant power supplies


Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: