Is it possible to connect the input power cable from the bottom on a wall mounted EVlink Pro AC Metal ?
No, we cannot connect a wall mounted EVlink Pro AC Metal from the bottom because there is a metal cover. The connection can only be done from the top or from the side.
Released for:Schneider Electric Nigeria
Explore more
Range:
EVlink Pro AC
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.