{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to get the firmware version of a M580 CPU (BMEx58x0x0 or BMEx58x0x0S) ?

If the firmware has never been updated since it has been manufactured, the SV marked on the product shows the firmware release set inside the module.

Otherwise, there are several methods for getting the firmware release of a M580 CPU :

1 : By connecting Control-Expert to the CPU :
a.1 : Connect Control-Expert to the M580 CPU
b.1 : double click on the CPU in the configuration screen or open the
c.1 : the version is displayed on top of the window as show below :
SV M580
Or
a.2 : Connect Control-Expert to the M580 CPU
b.2 : Open the PLC screen (Alt+7)
c.2 : Open the sheet "Information" in the PLC Screen window
d.2 : Select the PLC->IDENTIFICATION menu
e.2 : The firmware release appears under the parameter "PROCESSOR VERSION" :
M580 SV PLC Screen

Note : first digit displays the major version (3 in the example), second digit displays the minor version (20 in the example), and for M580 Safety only, third digit displays the major version of the Coprocessor (5 in the example). The last digit is the Internal Release (for internal use only).
2 : By using Unity-Loader software tool (SV<4.01 only):
a : Connect Unity-Loader with the CPU (either through USB or Ethernet) and click on "Connect" button
b : the firmware release is displayed on the right window as shown below (version 3.20 in our example for the CPU and, for M580 safety only, version 5.01 for Coprocessor) :
unity loader CPU
3 : By using EADM (EcoStruxure Automation Device Maintenance) tool :
a : Connect the tool with the device selecting :
  • "FTP" or "USB" connection (for firmware <=3.20) (FTP service should be enabled inside the embedded application)
  • "HTTPS" (for firmware >=4.01) (HTTP service should be enabled inside the embedded application)
connect eadm

b : Select the package (*.ldx file or *.eadp) available in the "Data Package" folder :
eadm slect
c : Click on the icon to enter the Firmware password and click on Connect => the firmware version of the device appears in the box (in this example, 3.20)
pass2
Note : For firmware version higher than 4.01, cybersecure mode will add some additional constraint which could differs from the steps described above (but still unknown at the creation of this FAQ)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: