{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I diagnose the channel and module status of the BMEAHI0812 and BMEAHO0412 Hart modules
Issue:
Diagnostic LED for the BMEAHI0812 and BMEAHO0412 Hart modules


Product Line:
BMEAHI0812, BMEAHO0412


Resolution:
Use the combined states of the RUN, ERR, I/O, BS, An and Hn LEDs to diagnose the channel and module status for the BMEAHI0812 and BMEAHO0412 modules:
Hart

Hart2

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: