Search FAQs
What is the minimum version of EcoStruxure Control Expert needed to configure the PMEPXM0100 Profibus module?
Issue:
Minimum version of EcoStruxure Control Expert needed to configure the PMEPXM0100 Profibus module
Product Line:
Control Expert, PMEPMX0100
Resolution:
The minimum version of EcoStruxure Control Expert needed to configure the PMEPXM0100 Profibus module is V14.0 with the installation of hotfix ControlExpert_V140_HF_PMEPXM0100
Minimum version of EcoStruxure Control Expert needed to configure the PMEPXM0100 Profibus module
Product Line:
Control Expert, PMEPMX0100
Resolution:
The minimum version of EcoStruxure Control Expert needed to configure the PMEPXM0100 Profibus module is V14.0 with the installation of hotfix ControlExpert_V140_HF_PMEPXM0100
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: