{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
SchneiderElectric_KBA_Basic_Meter_PM55xx Russian Language files issue
SchneiderElectric_KBA_Basic_Meter_PM55xx Russian Language files issue

Problem statement :

Pm5560 Meter set to Russian language, the Panel data is not visible and some of data labels are not visible in different screen navigations.
Russian Language issue

Causes identified :
  • This data label missing or data missing in PM55xx is identified when Meter is set to Russian language.
  • This is due to some issue with the Russian language file used within PM55xx.
  • This issue is noticed with Pm55xx with firmware versions below 4.1.3

Solution :

Schneider Electric Nigeria

Attachment(s)
SchneiderElectric_KBA_Basic_Meter_PM55xx_Russian_language_Issue.pdf [347.55 KB]