{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I update the M580 CPU’s firmware via the BMENOC03xx module?
Issue:
Firmware update the M580 CPU’s firmware via the BMENOC03xx module


Product Line:
M580


Resolution:
Yes, you can connect the BMENOC03xx module’s embedded Ethernet switch to the CPU. Check that the BMENOC03xx module is running properly before starting the update procedure.
You cannot, however, update the CPU if Unity Loader is connected on the BMENOC03xx module’s IP address.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: