{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the purpose of the Transfer Tool that is installed with EcoStruxure Machine Expert Basic?
Issue:
Purpose of the Transfer Tool that is installed with EcoStruxure Machine Expert Basic


Product Line:
EcoStruxure Machine Expert Basic


Resolution:
The Transfer Tool is a console application allowing scripting operations without using EcoStruxure Machine Expert - Basic.
The Transfer Tool allows you to:
  • Download and upload the project to and from the controller.
  • Update the controller firmware.
  • Backup and restore application data.
NOTE: To use the Transfer Tool, you must connect the PC to the controller using a USB cable.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: