{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I upgrade the firmware of a BMEAHI0810 module with a PC located on the Control Network of the BMENOC0321 ?

The gateway address of the BMEAHI0810 module should be the IP address of the fieldbus network of the BMENOC0321.
For instance , below the Ethernet network Manager screen of my application where the gateway of my AHI is the IP address of the router :
BMEAHI0812, Gateway,BMENOC0321

In the BMEAHI0812 DTM instance, you need to enable the option "Firmware upgrade"  as follow :

EnableFirmwareUpgrade

And always perform a transfer to FDR server after each modification of the BMEAHI0812 DTM instance.
Then open Unity Loader and connect to the IP address of your BMEAHI0812 module to perform the upgrade :
BMEAHI, upgrade,Unity Loader

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: