{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Network Management Card 4 – EAPoL configuration procedures from Web UI/CLI
Issue:
EAPoL configuration from the Web UI/CLI in the Network Management Card (NMC) 4.

Product:
Galaxy VL – Built-in Network Management Card 4 and AP9644.

Environment:
NMC firmware - Galaxy VL 10.11.0

Solution:
The Network Management Card (NMC) 4 EAPoL configuration differs from the NMC 2 and NMC 3 so you may need to check the below points before configuring EAPoL on the NMC 4.
  1. The CA certificate and the user certificate must have a file extension of “.crt” in PEM or DER format.
Note: The NMC 4 accepts both: PEM and DER formats. We recommended using the PEM format for both the user certificate and its corresponding private key. The user’s certificate and its private key must be in the same format for the EAPoL authentication to be successful.
  1. In the Web UI, the certificate validation occurs after entering the passphrase, loading the CA certificate (ca.crt), private key (user.key), and user certificate (user.crt).
  2. EAPoL can be forced to re-authenticate by using the ‘eapol -r’ Command Line Interface (CLI) command.
  3. An empty passphrase is set via the CLI using ‘eapol -p “” ‘
  4. To support a private key (user.key) that isn’t password-protected, enter an empty passphrase.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: