{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there any settings needed to run a ATS22 soft start on a Corner Grounded Delta System?

Issue:

Settings needed to run a ATS22 soft start on a Corner Grounded Delta System.

Product Line:

ATS22

Environment:

Corner-Grounded Delta system

Cause:

n/a

Resolution:

When you have a corner grounded system on the ATS22, DO NOT change the DETLA settings in the config menu, leave it as LINE.

Would also suggest to go CONF menu and set LAC to on and then go to the ADJ menu and turn the SSC to off.

Schneider Electric Nigeria