{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which access point wifi or 4G router can be recommanded for Harmony Edge Box HMISTM6BOXIOT?
The goal of this FAQ is to propose some recommanded architectures using access point wifi / 4G to connect HMISTM6BOXIOT to the cloud, EcoStruxure Secure Connect Advisor or display the hardware configuration & Mobile Access of EcoStruxure Machine SCADA Expert.

This article is applicable for HMISTM6BOXIOT + EcoStruxure Machine SCADA Expert 2020 SP2 (minimum).

Architecture 1: Access to Mobile access and Hardware configuration through Router Wifi Teltonika RUT240 (wifi or 4G).
architecture 1

Architecture 2: Access to HMISTM6BOXIOT remotely through EcoStruxure Secure Connect Advisor with router Teltonika RUT240.
architecture 2

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: