{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I setup an XBTF Magelis HMI to communicate to a M340 serial port via RS232?
Issue:
XBTF communication to a M340 serial port via RS232


Product Line:
XBTF, M340


Resolution:
For RS232 communication between the Magelis XBTF and M340 PLC, the cable pinout should be as follow:
image

The M340 serial port must be configured for RS232 as shown below
image2


The XBTF configuration should match the serial port setup of the M340.
image1

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: