{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the category Class of EVlink Pro AC ?
EVlink Pro AC is class 1, because of earth connection
IEC 61851-1:2017-02 mentions in §5.6 Protection against electric shock the equipment shall be classified according to the protection against electric shock
NOTE Class descriptions can be found in IEC 61140:2016, 7.3, 7,4 and 7.5.)
In IEC 61851-1 : 2017

Schneider Electric Nigeria