{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How must I configure OPC UA communications when an IPSEC tunnel is configured?
In the case where secured OPC UA client connect to the BMENUA server and IPSEC tunnels are activated to the clients, by default the OPC UA connections will pass inside the tunnel. For the best performances, we recommend configuring the product in order to pass these OPC UA connections outside the tunnel. This can be done as following:
  • ADD a new FORWARDING rule,
  • Select OPC UA protocol,
  • Inbound interface CONTROL PORT or BOTH,
  • uncheck IPSEC in use in order to force OPC UA traffic to pass outside the IPSEC tunnel  

Product Line

BMENUA0100 version 2.01

Environment

Windows, EADM
 

Schneider Electric Nigeria

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.