{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Power SCADA Operation: IO Server is crashing for the IEC870IP (IEC104) Device

Issue
After starting runtime server, IO Server process is crashing which is configured with IEC104 protocol device.

Environment
Power SCADA Operation (PSO) 2020
EcoStruxure Power Operation (EPO) 2021

Cause
Blank cell in IOA configuration file (IECIOA.dbf) for a configured IOA of type ‘DDO’.
IECIOA

Resolution
Make sure to configure IECIOA.dbf file properly (in case of any doubt refer driver help) and make sure that for the output tags/points cell values of all columns in the config file is mandatory and must be configured. For other than output tags, column’s TYPE, QUALIF, SELEX cell values are optional and can be left blank.

Schneider Electric Nigeria

Power SCADA Operation: IO Server is crashing for the IEC870IP (IEC104) Device

Issue
After starting runtime server, IO Server process is crashing which is configured with IEC104 protocol device.

Environment
Power SCADA Operation (PSO) 2020
EcoStruxure Power Operation (EPO) 2021

Cause
Blank cell in IOA configuration file (IECIOA.dbf) for a configured IOA of type ‘DDO’.
IECIOA

Resolution
Make sure to configure IECIOA.dbf file properly (in case of any doubt refer driver help) and make sure that for the output tags/points cell values of all columns in the config file is mandatory and must be configured. For other than output tags, column’s TYPE, QUALIF, SELEX cell values are optional and can be left blank.

Schneider Electric Nigeria

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range: