{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the compatibility between application and software version for a Premium PLC when opening the .STA file?
Issue:
Compatibility between application versions and software versions for Premium PLC platform


Product Line:
Premium, Unity Pro, EcoStruxure Control Expert


Resolution:
The table below gives the compatibility between application versions and software versions:
Premium

Note: with restrictions below:
  • When an .STA file created with Control Expert or Unity Pro ≥ V7.0 contains extracted bits in DDT, the .STA file cannot be opened with Unity Pro version < V7.0.
  • When an .STA file created with Control Expert V15.0 Service Pack 1 or later is protected with the file encryption option, the .STA file cannot be opened with Control Expert V15.0 Classic and earlier.


Schneider Electric Nigeria