{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV212 Undevoltage Level in Amps or percentage.
Issue:
Why does F611 parameter for ATV212 shows Amps in SoMove but the manual shows percentage(%)?

Product Line:
ATV212, S-Flex

Environment:
All

Cause:
NA

Resolution:
When F610 (Underload Detection is enabled, F611 can be adjusted in Amps or Percentage(%) depending upon F701 setting.
F611= underload level is in A or amps (Factory Default). If you change F701 to 0 you can set this as a % of the Drives IN current ratings.

Schneider Electric Nigeria