{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the EcoStruxure OPC UA server Expert allow dynamic IP address of the computer without a repair setup for the certificate update?


Issue:
Dynamic IP address for OPC UA Server Expert


Product Line:
EcoStruxure OPC UA Server Expert


Resolution:
Yes, The OPC UA server will support the use of dynamic IP address by way of the /dynamicip command line parameter.. This allows the server to ignore IP address machine modification that would require a setup repair for certificate update. This will help to manage certificates with dynamic IP.  To allow dynamic IP, run the command OPCUAServerExpert.exe /dynamicip.

Schneider Electric Nigeria