Search FAQs
Does Ecostruxure control Expert support HVAC library?
Issue:
HVAC library for EcoStruxure Control Expert
Product Line:
Ecostruxure Control Expert
Resolution:
Yes. The HVAC Library function blocks can be used on PLCs of the Quantum, M340 and M580 product family. Ecostruxure Control Expert V15.1 and above is required.
The following are the list of derived function blocks family wise which are available in this release of library.
EcoStruxure Modicon Libraries – HVAC 2022 can be downloaded from the link below
https://www.se.com/ww/en/download/document/MODICONHVAC2022/
HVAC library for EcoStruxure Control Expert
Product Line:
Ecostruxure Control Expert
Resolution:
Yes. The HVAC Library function blocks can be used on PLCs of the Quantum, M340 and M580 product family. Ecostruxure Control Expert V15.1 and above is required.
The following are the list of derived function blocks family wise which are available in this release of library.
EcoStruxure Modicon Libraries – HVAC 2022 can be downloaded from the link below
https://www.se.com/ww/en/download/document/MODICONHVAC2022/
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: